Hello Team,
My customer intend to use TLV733P as 3.3Vin to 1.2Vout 165mA, it has Vdrop=2.1V and power dissipation is 0.3465W, they are wondering if TLV733P X2SON (4) package can support 346.5mW?
The datasheet only mentioned 300mA is max recommended, but it doesn't mention max power dissipation.
What can you tell about the max power dissipation fo TLV733P?
If TLV733P X2SON (4) package can support 346.5mW?
Thanks.
Martin