What is the output voltage accuracy at 1.5V? Datasheet says +/- 40mV for <1.5V and +/- 2% at 1.5V to less than 2V. At 1.5V, 2% does not equal 40mV. This happens at 2V. Customer is operating at 1.5V.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the output voltage accuracy at 1.5V? Datasheet says +/- 40mV for <1.5V and +/- 2% at 1.5V to less than 2V. At 1.5V, 2% does not equal 40mV. This happens at 2V. Customer is operating at 1.5V.
Customer is asking:
How can we tighten this up from the +/-3.33% @1.2Vout to +/- 2% or better?
Is this over all line/load conditions or part variation?
For our application we most likely will not exceed 250mA with a 3.3V supply at 1% +2% ripple feeding this 1.2 LDO.
The largest transient is ~180mA, from ~60mA to ~240mA
Originally we were using LP5907MFX-1.2/NOPB not much margin/growth.
Hi Ronnie,
For the original question, the 1.5V output has a specified accuracy of ±2%. This line specifies Vout greater than or equal to 1.5V. The ±40mV line specifies Vout less than 1.5V.
The dominant source of inaccuracy is the reference voltage. As such the accuracy will not improve significantly with a lower load as seen in Figure 6.
Very Respectfully,
Ryan