Part Number: TPS7A8001
Hello,
In the customer, the output voltage is oscillated at the middle voltage when the input voltage is slowly dropped.(3.3V to 1.0V/10ms)
Vin =3.3V, Vout =1.5V, Iout=95mA
The oscillation is occured when Vin is 1.9V and Vout is 1.2V
EN pin is connected to Vin
The phenomenon does not occur if the load is increased or the input voltage falls fast.
Could you please let me know this operation reason?
Is there a possibility that this behavior will damage the device?
I can send the waveform and schematics if you contacted to the following e-mail address.
asaka-r@clv.macnica.co.jp
Best Regards,
Ryuji