Hi,
I am currently working on the TPS7A4001 in a design. The datasheet has been respected as shown in the figure below. The component is working with the following caracteristics:
Vin=49V
Vout=5V
Iout=16.3mA
In spite of this, the component's temperature sometimes goes up to 126°C and I can't figure out why. I tried to use greater Cin and Cout but in vain. I removed the load and inserted a simple resistor but the result didn't change. Any ideas of the issue? Are there any recommendations for current input values?
Thank you,
Fabien