Hi Sir/Madam,
Please help to advise on the issue. There is unexpected voltage drop when load applied. The input voltage is 12V and the output voltage is 7V, connected to load circuit through a long wire.
The expected output voltage, 7V is obtained when it is not connected to the load circuit. Unexpected voltage drop to 2.4V when the load circuit connected. Please refer to the circuit for the LM1084 and load circuit as attachment.
Hope to hear from you soon. Thank you very much.