Hi.
I have a question regarding the output capacitors connected to a LP2951-N, where the datasheet have different statements:
- Paragraph 8.3.7 (page 17) says, that the output capacitor can be a ceramic type with a ESR down to 6 mOhm
- Paragraph 9.2.1.2.1 (page 20-21) says than an ESR of app. 5 Ohm is needed, and an extra resistor must be added in series with the output capacitor.
What is right and what is wrong? Can the LP2951-N run stable with just a ceramic output capacitor, or is an extra 1 - 2 ohm serial resistor needed?
The datasheet is marked "SNVS764P –JANUARY 2000–REVISED MAY 2016"
Best regards
Niels Ole Jorgensen