TPS7A85A: Temperature characteristic

Part Number: TPS7A85A

Hi

My Customer has question.

Can you tell me the thermal resistance between "junction TJ" and "ambient temperature TA" at forced air cooling 1 m / s?

Assuming worst case, load current 3.9 A, voltage difference 0.326 V, ambient temperature 75 ° C., forced air cooling 1 m/s.

I want to check if it can operate under this condition.


I think that it is difficult to deal with, but I want comments.

Best Regard

T Kishi

4 Replies