This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

maximum Iq of TPS7B63-Q1

I have a question about TPS7B63-Q1.

Please tell us the maximum Iq under the following conditions.

  Vin=14V

  Vout=3.3V

  Iout=20mA

Best regards,

Takahiro Nishizawa

  • Hi Takahiro-san,

    The max Iq for those conditions would fall under the 3rd line of the Iq specification it is circled below. This maximum may be higher than what you see in your system as it covers up to 100mA of load current. You can estimate the maximum using Figure 1.

    Best Regards,
    Mark

  • Hi Takahiro,

    From the Electrical Characteristics (EC) table, max Iq for Iout < 100 mA is 98 uA. and max Iq for Iout < 1 mA is 42 uA.

    If we extrapolate linearly, I would estimate max Iq for Iout = 20 mA at about 52 uA.

    I will check to see if we have test data at Iout = 20 mA

    Best,
    Eric Preiss | Applications and Validation Engineer | Linear and Low Dropout Regulators | Texas Instruments

  • In reply to Eric.Preiss:

    Thank you for your answer!

    I am waiting for test data at Iout=20mA.

    Best regards,

    Takahiro Nishizawa

  • In reply to Takahiro Nishizawa:

    Thank you for your answer!

    Do you have the test data at Iout=20mA?

    This is big project(500k/Y)!
    The IC is used in the sensor of car doors.

    We are waiting fot your quick response.

    Best regards,

    Takahiro Nishizawa
  • In reply to Takahiro Nishizawa:

    Hi Takahiro-san,

    I'm sorry, we do not have test data available for max Iq with Iout=20mA.

    Best,
    Eric Preiss | Applications and Validation Engineer | Linear and Low Dropout Regulators | Texas Instruments

  • In reply to Eric.Preiss:

    Thank you for your answer!


    Our competitor is RICOH R5112.
    Maximun Iq of R5112 is 9.8μA(Iout=0mA)
    We need to explain that Iq of TPS7B63-Q1 is lower than R5112.

    I have another questions.

    Question 1.
    Please tell us the test condition and the test limit about Input quiescent current in datasheet p.6
    when Vin is 14~40V.

    Question 2.
    About Figure .1 in datasheet p.8,
    do you have evaluation data when Vin is 14V and Ta is 25℃ and 125℃?

    Best regards,


    Takahiro Nishizawa
  • In reply to Takahiro Nishizawa:

    Hi Takahiro-san,

    The RICOH R5112 datasheet specifies max Iq of 9.8 uA with Iout = 0 mA.
    The closest spec in the TPS7B63-Q1 datasheet is Iq with watchdog disabled and Iout < 1 mA: 29.6 uA max.

    Please note the TPS7B63-Q1 has a watchdog function, while the R5112 does not have watchdog.

    Q1) Test Condition: 4 V, 14 V, 40 V, no watchdog, Iout = 0.2 mA.
    Test limit is 29.6 uA

    Q2) 14 V, Iout = 0.2 mA, Iq max @
    25°C = 20.0735 mA
    125°C = 22.3631 mA

    Best,
    Eric Preiss | Applications and Validation Engineer | Linear and Low Dropout Regulators | Texas Instruments

  • In reply to Eric.Preiss:

    Hi Takahiro-san,

    I had a typo in my last post.

    Q2) 14 V, Iout = 0.2 mA, Iq max @Q2) 14 V, Iout = 0.2 mA, Iq max @
    25°C = 20.0735 uA
    125°C = 22.3631 uA

    Best,
    Eric Preiss | Applications and Validation Engineer | Linear and Low Dropout Regulators | Texas Instruments

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.