Shootup voltage observed at the output of LP3997.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Shootup voltage observed at the output of LP3997.
Hi,
i already checked taht with 1-2sec, it is working fine.
What is the issue with 200ms.?? My use case is with 200ms..
Regards,
Gautam
Hi Gautam,
Thanks for the update. Since the issue is gone when you slowed down the cycles, we can confirm the overshot is due to the fact that between Vin cycles, the internal reference voltage is not being fully discharged. Essentially the overshot is due to the device startup when the internal reference is not zero. During normal startup, Vin is proportional to internal reference. But when internal reference is not zero, the unbalanced loop will try to pull vout high to catch up the non-zero internal reference.
Since there is no external connections for you to discharge the internal reference voltage, unfortunately you will need to slow down your Vin cycle to prevent excessive overshot due to startup with unbalanced loop.
Regards,
Jason Song