Q: TPS7A4533 ESD by 3276

need ESD data for TPS7A4533DCQ. Needs to confirm it’s ok to be built in factory with ESD control standard 100V

1.      Human Body Model

2.      Machine Model

3.      Component Device Model

Thanks and regards,


A: Re: TPS7A4533 ESD by 10449

Texas Instruments power products meet an ESD rating of at least

Human Body Model ( HBM ) > 2000V

Charge Device Model ( CDM ) > 500V

TI does not specify the Machine Model

 

Any IC with lower ESD ratings that stated above will state the actual rating in the datasheet.

 

 

( ESD ESD  ESD ESD ESD rating, ESD rating, ESD rating, HBM, HBM, Human Body Model )