This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS63070
Hello,
In the datasheet, we can see the accuracy for TPS63070, but TPS630701(fixed 5Vout version) is not shown.
Could anyone provide the Vout accuracy value or data for TPS630701 ?
Thanks,
Hiro
In reply to Sabrina:
Hello Sabrina-san,
The customer thinks that TPS630701 Vout accuracy is a little bigger than TPS63070(1% in PWM mode and 3% in F|PFM mode)
due to internal divider resistors. (Is the accuracy of TPS63070 not include external divider resistors accuracy, right ?)
And they cannot decide whether their thought is collect or not by Fig.38 and 39 of the datasheet.
The application is some FA equipment (detail is not cleared so far).
Thanks and best regards,
In reply to Hiroshi Sato:
I will check with the designer and get back to you
Thank you for replying, I'll tell that the customer.