• Resolved

TPS54302: About Overcurrent Protection

Part Number: TPS54302

Dear experts, the TPS54302's maximum continuous output current is 3A. When the load current is 3.5A, what will happen? TPS54302 will turn off? If the TPS54302's output is short to GND, what will happen? TPS54302 has short-circuit protection and over current protection function? If this error conditions last for long time, the TPS54302 will be damaged? Or, The TPS54302 will restore to normal state when the error condition is removed? How can I calculate the exact output current that will shutdown the TPS54302? Thanks.