This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TPS61021A: is this ic suitable for my application?

Part Number: TPS61021A

Dear Sir,

I have design inquiry:

Vin=1V ~ 3V

Vout=3.8V

Iout_peak=2.3A(the peak current sustain time is about 580us)

Iout_average=200mA

I looks up in your website and i find TPS61021A looks like suitable for my applicaiton.But i am not very sure.

So, could you help to give me some advise?

Thanks. 

  • Vin=1V is too low. if Vin is higher than 2V, then it can support this case.

    Best Regards,
    Helen

    Boost DC/DC Solution

  • In reply to Helen chen:

    Hi Helen:
    Does TI have some solution for my design?
    Or, could i use big capacitor at TPS61021A 's output pin to solve this issue?

    Thanks.
  • In reply to Matthew.huang:

    1V inpus is too low, even big can't help. if the 1v input is a must,  then you can refer to the TI design PMP9772.

    Best Regards,
    Helen

    Boost DC/DC Solution

  • In reply to Helen chen:

    Hi Helen:

    Thanks for you reply.

    But if i decrease the RF PA current to 1.8A, is TPS61021 ok?

    And how do you caculate the peak current 's relationship with input voltage? Could you show me the formulation?

    Thanks.
  • In reply to Matthew.huang:

    If your min input voltage is 1V , then the maximum output current is less than 1A.   So still not fit.

    Isw_valley=Po*(1-∆IL)/(eff.*Vin)

    Best Regards,
    Helen

    Boost DC/DC Solution

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.