• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Power Management » Non-Isolated DC/DC » Non-Isolated DC/DC Forum » TPS63020 PS/SYNC and VINA Connections
Share
Non-Isolated DC/DC
  • Forum
  • E2E Wiki
Options
  • Subscribe via RSS

TPS63020 PS/SYNC and VINA Connections

TPS63020 PS/SYNC and VINA Connections

This question is answered
Shlomi Yehezkia
Posted by Shlomi Yehezkia
on Jun 21 2011 05:27 AM
Intellectual450 points

Hi,

Q1: Can the PS/SYNC pin (power safe mode) be active for good?

 

Q2: Should the VINA pin be also connected to VIN or is it internal connected?

 

Q3: from page 12 from the PDF file it seems that there are six capacitors, from the layout point of view (page17) there are additional two more capacitors.

Please send me TI recommended application notes for Vout-5V

 

Please find Q4 regarding the GND and power ground of the TP63020 and bq24020.

Q4: the charger bq24020 powers up (VIN) the SPS TP63020. Can the charger ground be the same plan as the SPS GND pin 2. In all hoe should the ground separation between the two IC be like. A sketch will be fine.

Thanks,

Shlomi

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Daniel Acevedo
    Posted by Daniel Acevedo
    on Jun 22 2011 11:28 AM
    Verified Answer
    Verified by Daniel Acevedo
    Genius16890 points

    Generally, we recommend you follow the design procedure in the datasheet and your schematic and layout match that of the EVM. 

    See my comments below:

    Shlomi Yehezkia

    Q1: Can the PS/SYNC pin (power safe mode) be active for good?

    [D.A.] PS/SYNC is an input to enable power save mode or for a system clock. Per the description on page 13 of the datasheet, grounding this pin allows the converter to enter power save mode at light loads; pulling this pin high forces the device to remain in PWM mode for all loads. Or instead, a system clock can be applied between 2.2MHz and 2.6MHz to synchronize multiple power supplies. 
    Did you mean output PG (power good) pin? PG, open-drain output, should have a 1 M Ohm pull-up to Vout and is '1' when power is good and '0' otherwise. 
    Q2: Should the VINA pin be also connected to VIN or is it internal connected?
    [D.A.] VINA should be connected to a 0.1uF ceramic capacitor. VINA has an internal connection to VIN and does not need to be externally connected to VIN. 
    Q3: from page 12 from the PDF file it seems that there are six capacitors, from the layout point of view (page17) there are additional two more capacitors.
    [D.A.] The additional pads on the layout are un-populated and are available to add more input/output filtering capacitors.  
    Please send me TI recommended application notes for Vout-5V
    [D.A.] To design for Vout = 5 V, you will need to also specify Vin and at least your output current. You can follow the design procedure in the datasheet and use Switcher-Pro free design software to aid in the design. 
    Please find Q4 regarding the GND and power ground of the TP63020 and bq24020.
    Q4: the charger bq24020 powers up (VIN) the SPS TP63020. Can the charger ground be the same plan as the SPS GND pin 2. In all hoe should the ground separation between the two IC be like. A sketch will be fine.
    [D.A.]  No. The BQ24020 charger needs to be connected to power ground of the TPS63020. The TPS63020 Pin 2 GND should be connected TO PGND only under the IC.

     

    vin PGND GND TPS63020 TPS63011 tps63010 VINA TPS6302x TPS6301x TPS6303x TPS63021 PG PS/SYNC
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Shlomi Yehezkia
    Posted by Shlomi Yehezkia
    on Jun 23 2011 06:37 AM
    Intellectual450 points

    See my comment in red

    Generally, we recommend you follow the design procedure in the datasheet and your schematic and layout match that of the EVM. 

    See my comments below:

    Q1: Can the PS/SYNC pin (power safe mode) be active for good?

    [D.A.] PS/SYNC is an input to enable power save mode or for a system clock. Per the description on page 13 of the datasheet, grounding this pin allows the converter to enter power save mode at light loads; pulling this pin high forces the device to remain in PWM mode for all loads. Or instead, a system clock can be applied between 2.2MHz and 2.6MHz to synchronize multiple power supplies. 

    Did you mean output PG (power good) pin? PG, open-drain output, should have a 1 M Ohm pull-up to Vout and is '1' when power is good and '0' otherwise. 

     

    During my operation my system can encounter low loads (100-200mA) and high loads (1A- during transmissions), so in order to exceed high efficiency at  low and high loads, can the PS pin remain low for such application.?

     

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Daniel Acevedo
    Posted by Daniel Acevedo
    on Jun 23 2011 09:37 AM
    Verified Answer
    Verified by Daniel Acevedo
    Genius16890 points

    If you connect PS/SYNC low, the TPS63020 will automatically transition between power save mode and PWM mode as the load varies. 

    In your case, where the load is always greater than 100 mA, the TPS63020 will not enter power save mode; however, at 100-200 mA loads the efficiency of PWM mode is still relatively high (greater than 80% if you follow the design and layout of the EVM).

     

    Efficiency TPS63020 PWM Power Save PS/SYNC
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use