I am testing a new design using the TPS61222 to generate 5V from a 2AA battery pack. The 5V rail is only required for a subsystem containing LEDs - the MCU runs directly off the battery. When the regulator is enabled in order to supply power to the 5V subsystem, an inrush current of up to 200mA is possible as the output cap charges. This causes the battery voltage to drop to the point where the MCU could be reset, even from a moderately low battery.
I noticed that the TPS61222 info page (http://www.ti.com/product/tps61222) links to an application note about addressing this exact problem with the TPS6107x family of converters (http://www.ti.com/lit/an/slva307/slva307.pdf). The soft start circuit described in this application note seems like it could be used on the TPS6122x family as well, especially if I switch to the adjustable voltage version TPS61220, which gives access to the feedback network. However, the internals of the two converter families are a bit different.
Can I apply the soft start technique for the TPS6107x to the TPS61220? What about techniques to limit the inrush current in the fixed-output TPS61222?
Thanks,
Ryan