This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62410 EVM available?

Guru*** 143870 points
Other Parts Discussed in Thread: TPS62410, TPS62420

Q: Is there a TPS62410 EVM orderable on the web?

 A:  No but the TPS62410 and TPS62420 have the same package and pinout.  Therefore, you can remove and replace the TPS62420 IC on the TPS62420EVM-167 with a TPS64210 IC.  Note that the inductor on TPS62420EVM-167 may not be rated high enough for an application using the TPS62410 and so the inductor may need to be replaced.  There are no plans to develop a dedicated EVM for the TPS62410.