We've a design using the LM25011 as the first regulator stage - 24Vdc nominal input, 14V output. The prototype works fine but the LM25011 has failed during EMC Approvals Testing. This was whilst testing for Conducted DC Immunity - 11V of common mode RF applied to the +24V and 0V input lines simultaneously (simulating a radio signal nearby). During this test the regulator circuit failed, ceasing to put out any output voltage. The circuit did not recover. The IC has been replaced and indeed was the faulty component, but on re-test it again died.
The (core of the) circuit was generated by WEBENCH. Would be grateful for any feedback on how/why the IC would be terminally damaged by this test (and possible fixes!)
Thanks