Hi,
We are using TPS54360 DC-DC Converter in one of project that will be implemented in Automotive Envoronment with following specification.
Working Voltage = 24V.
Output Voltage = 5V.
Average load current = 300 mA.
Switching Frequency = 700 Khz.
I have observe some Load dump surges at the at the vehicle Battery with following specifications.
Pulse Time period = 350 msecons.
Pulse peak voltage = Around 80V.
In datsheet of TPS54360 it is mentioned that Max Input voltage is 65V.
If I apply 75V for the period of 350msecond then will it damage TPS54360 ?
In other words , Can anybody specify the Surge handling Capacity of TPS54360 ?
Thanks in advance.
Regards,
Rajesh Matere.