Hi all, I am trying to find the source of erratic dropouts in a somewhat specialized dc/dc application. I have 8 LM5085s on one pcb, 48V input, outputs vary but most are in the 40V/200mA range, one is 30V/700mA and another is 44V/800mA.
The 44V/800mA is particularly troublesome.
The design right now has 2.2K in parallel with 1000pF for the current limit "ADJ" (pin 1) and at 0.05R sense resistor that the ISense (pin5) goes to. This should give me a current limit of 1.76amps, way more than needed.
In this application I would like to disable the current sense, as well as the overvoltage output protection (i.e. if FB is > 1.6V).
If I replace the current sense resistor with a wire, I would expect to never have the current limit trip. Instead it trips continuously. If I replace the current sense resistor with 0.15ohms, i.e. 0.6amps, which is definitely below the current draw when the inductor is charging up, it works fine.
Any ideas appreciated.
J