Hi,
My customer would like to use TPS61175 with following condition.
[Condition]
-Input Voltage (Vin) =7.0V
-Output Voltage (Vout) =12V
-Output current (Iout) = 1.0A
-Load capacitor (Cload) = 3300uF
-Soft Start capacitor (C3) = 1uF to 4.7uF
They are going to use the large C3(1uF to 4.7uF) to control the rush current.
Please let me know the following questions.
- What is the maximum value for C3?
- Do you have the calculating formula of the soft start time (Tss)?
Regards,
Kanemaru