Hello,
Please answer following question from customer.
Q1:
Datasheet P27 has following equation.
-Please advise what is the 30%.
-Explanation is “The peak-to-peak ripple is limited to 30% of the maximum output current.” so equation should be ILip(max)=0.3 x Iout(max).
Please advise if equation (34) is correct or not, and what is “Iout(max)/(1-Dmin)”.
Q2:
Datasheet P28,29 has following equation.
These equations have constant 8, 7/8, 4 and 2.
Please explain meaning of each constant.
Please advise if these constant should be changed depend on capacitor type or always use 8, 7/8, 4 and 2.
Best Regards.