Dear Sir/Madam,
I am experiencing 400mV pk-pk output ripple when the LM5116 is used to convert +48V to +12V@8A.
The amplitude of the ripple is pretty consistent when the output is swept from 1A to 8A with an eLoad.
The circuit was designed using web bench with a change to the FETs due to availability.
The FETs do not get as hot as the inductor which sits at around 65-70 degrees.
The circuit can be found:
Q1. What could be causing the 400mV pk-pk ripple and can this be improved?
Regards Grant