Hi,
I want to use the Output over-voltage protection of the TPS61260DRV as a regulating process in my application. I set the output voltage above 4.5 V with the divider (Rp8, Rp9) and charge the ultra-capacitor with a 100mA current set by Rp5. The converter works only when the Cp6, Cp7 voltage is lower than the protection voltage, When the voltage triggers the protection the IC enters shutdown state and takes only 9...11 uA from the battery. It works well for my application but I don't know if it's good for the IC. A few hours of testing passed normally without deviations. Can I use this IC in this mode?
Ilya