Hi,
I have a design with Vin = 32V and 3 LM25011 that regulate to 16V, 5V and 3,3V.
Calculating Rfb1 / Rfb2 give me :
- 16V -> 1k69 / 9k09
- 5V -> 4k99 / 4k99
- 3,3V -> 4k99 / 1k58
The 16V and 5V are OK, but 3,3V setup give me 2,58V... I have to change Rfb2 to 15k to have 3,3V approx... so 10 time bigger value than theorical !!!
For my 3,3V setup, I have put RT = 88k7 so FS = 800kHz, and Ton min = 126ns (>90ns) , Toff min = 1120 ns (> 15ns). L = 22uH. Cout = 47uF.
What possibly goes wrong for my 3,3V regulation ? Specially because 5V and 16V are all right, so my calculation should be good...