We have built a relay board with a dc/dc regulator LM25011, a relay and a buzzer.
The problem I have is that the voltage drops already after putting a 50ma+ load onto it. And if I put a 30ohm resistor across the output (Equals 180mA current draw) the voltage drops to 0.8V and it can't manage to pull it self back up.
We have looked over the design and can't find any misplaced components or anything.
Specs the regulator is designed for:
Input: 10V-30V
Output: 5V@1.5A
Inductor man.fact.nr: VLP8040T-220M
Attached is schematic and a picture of one of the assembled boards. Any help would be greatly appreciated.
Thanks.
-Fredrik