Hello Community,
We are using this buck converter in an application with a power demand of 15W peak and i have to find out which maximum ripple of the input voltage is acceptable.
The input voltage ranges from 7 to 42VDC and the input stage of the converter has two 10µF capacitors and transient protection.
The output voltage is set to 5V. It would be nice if you could provide me with a value or give me some hints how to calculate that by myself.
Best regards
Hannes