This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Design support on Part# LM5030

Other Parts Discussed in Thread: LM5030

Hi,

We need to design a DC to DC converter with following specification using TI Part# LM5030MM/NOPB

Input Voltage: 18V to 50V
Input Current: 30A Max
Output Voltage: 24V
Output Current: 20A

For this application we tried to get reference design from TI WebBench tool, but we are getting error saying "Your solution is not yet WEBBENCH enabled".
So please let me know how we can get design support for designing with this part.

Thanks & Regards,
Gopi krishnan K

  • Hi Gopi

    If you want to design a buck-boost convertor, I think you can't get suitable devices.

    However, I think you want to design a buck convertor from the device number(LM5030). In the case, you need to change the input voltage above output (24V). There are some devices of our company can be helpful. 

    Best Regards

    Feng Zhao