Hello,
I am designing a power supply with the following spec:
VIN = 4.2V to 50V
VOUT = 3.3V; LOAD = 200mA
I am using TPS54060 for this and Webench has suggested the attached design; I have chosen a capacitor with lowest values for capacitance & ESR from the suggested list of capacitors for this design.
4745.webench_design_670735_18_903927795.pdf
As I have to keep the output ripple to minimum, I would need to choose Cout with minimum ESR. With the current Cout, the phase margin is 37deg @ VIN = 50V; The phase margin is ~22degC at the lowest VIN. How could I improve that other than by increasing the Cout value?
Regards,
Sanjib