Hi
I would like to hear about TPS62750.
1. As long as I see figure 8, when output voltage is about 3.6V output current is from 0.6A to 0.7A, is Rlim_U 49.2kΩ at this time?
2. If input voltage is 4V or 5V, input current is 0.8A and Rlim_U is 30kΩ, does output current keep within 0.7A to 1.2A ?
Best regards!