This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

To decide R2 value of TPS62560

Other Parts Discussed in Thread: TPS62560

Dear All,

Would you tell us about the condition to decide R2 of TPS62560?
There is the following explanation in the datasheet P18 "OUTPUT VOLTAGE SETTING".
『To minimize the current through the feedback divider network,
 R2 should be 180 kΩ or 360 kΩ.』

■Can the customer not use the other resistance value for R2?
 (Can the user use 220kΩ for R2?)

Probably is it not a typographical error of "180kΩ - 360kΩ" ?

Best Regards
Tsuguhiko Asai