i'm so sorry, I want to ask what the componen that exact to convert +5V DC to negative 20 until 25 with current output min 500mA.., thank you everione who answer my questions...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What do you mean by "20 until 25"? You might look here for some ideas:
http://www.ti.com/lit/an/slva257a/slva257a.pdf
output voltage -20 until -25, i want to convert +5V dc to -20 until -25 DC, could you tell me, what the commponent that can i used. I used the LM2733 to convert +5v to +20V, it's very good, so i want the same componen that quality as goog as lm2733 but convert to -20..., can you help me??
You might want to look at TPS54340. There is an application note on inverting supplies here:
http://www.ti.com/lit/an/slva317b/slva317b.pdf
I'm sorry mr. Jhon, I was look for IC TPS 54340., but not it that I mean, not buck, but booster from 5Vdc to -20 until -24Vdc..., any solutions else??
That topology for +5 V input to -20 V output in inverting buck boost, not a boost converter which would take +5V input and be used to make a higher positive output. TPS54340 can be used for the inverting buck boost application as shown in the previously referenced application note. Am I missing something?