I am quite embarrassed, but I managed to make an incorrect symbol for the TPS63020. For the L1,L2,Vin and Vout I only use 1 pin of each pair of pins.
L1 = 8
L2 = 6
Vin = 10
Vout = 4
The feedback resistors are 768K and 137K to give 3V3
When the unit powers up, it does not seem to regulate, i.e. with input of 3V I needs to boost to 3V3 but it boosts to 4V7, causing high current draw from my 3V3 chips on the 3V3 rail.
My question is whether the chip will function like this, understanding that the current capability would be impaired. I can obviously modify the PCB to have these pins connected on the current boards, but it is a major mission to do.
Can an expert on the TPS63020 internals perhaps shed some light on my problem?
Regards
Ivor