Hi
Customer is mine is creating application of industrial tester.
To power supply camera subsystem they need to build circuit allowing to convert from 3.3V to 1,2V with 2A, Obstacle here is that this should be achieved 32kHz switching frequency which they want to achieve by selecting tight resistor RI.
As LM20143 has min frequency is 500kHz question is if they can reach required 32kHz and how this will implicate parameters, reliability and work life time of product.
Are you able to help to answer that question?