Regarding the TPS63050 and it UVLO.
Datasheet says it about 1.7V +- 200mV.
Also the min vin to keep output at rated current is 2.7V.
As a battery discharges (taking current), when exactly will the Vin input be disconnected.
approx. 1.7V or 2.7V.
Just trying to work out if this may cause damage to the lithium battery as it discharges?
Thanks