Hi,
i am using TPS63000 adjustable regulator to down-convert 3V from AAA battery (2 in series) to 2.7V for circuit operation. The circuit is designed exactly like the one in datahseet page#11 (http://www.ti.com.cn/cn/lit/ds/symlink/tps63001.pdf).
I am seeing high currents (more than 400mA to 1.2A) drawn by the regulator.. This behavior is very random since the current at most times is just 5mA. Since this is battery operated application, the cells heat up very quickly when this scenario occurs. The steel wire attaching the battery from holder to PCB heats up and has started melting the plastic enclosure.
As I said, this behavior is seen very random - happens once every 25 or so times. But, when this happens, the current stays high as long as the input is powered.
Another question was regarding R3 and C3 in the circuit in page#11. What is the use of this circuit? Can it cause the MOS gates to turn-on randomly during input transients? Is it only for power-on reset, similar to other devices which use this approach?
Regards,
Sriram V S