Hi Team,
My customer would like to use TPS61093 at the following condition.
[Condition]
Vin = 3.3V
Vsw = 3.0V to 4.6V (1cell battery)
Vout=12.4V
Iout = 20mA(max)
Could you please let me know about recommended rated voltage of flying capacitor (C3).
I believe that the rated voltage is 6.3V, because capacitor of this rated voltage is used on TPS61093EVM-519.
And, I have understood that they can use the capacitor of this rated voltage at all condition.
Is my understanding correct?
[TPS61093EVM-519 User’s Guide]
http://www.ti.com/lit/ug/slvu327/slvu327.pdf
Regards,
Kanemaru