Hello All,
I am working on a project where I will have the following requirements:
- Input: 0-36V
- Output: 3.8V
- Support up to 2A for GSM transmission
I used the TI Webench Power Designer to help me meet these requirements. It gave me a design using the LM3481 device. I have Implemented the design on my board but the Output is only 0.6V. I have triple checked all my connections to make sure there were no shorts or unconnected pins but I didn't find anything wrong.
Can someone help point me in the right direction? I have attached the schematic and layout of my design. I would appreciate any help that can be offered!
Thank you,
Anson N.