Dear TI
I'd like to know TPS40210 can work at below condition or not.
Vin=19V, Vout=120V, Io=0.5A
If you have reference design,. please let me know.
Customer is interisting in this device.
Thank you for your cooperations.
K.Narisawa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI
I'd like to know TPS40210 can work at below condition or not.
Vin=19V, Vout=120V, Io=0.5A
If you have reference design,. please let me know.
Customer is interisting in this device.
Thank you for your cooperations.
K.Narisawa
Webench says it can be done to your specification. There are quite a few reference designs using TPS40210. I did not see one that exactly meets your requirements.
Hi John-san,
Thank you for your kindly support always.
I also checked it out too.
I'll check customer how marginal do they have for this spec.
Thank you so much.
Best Reagrds
K.Narisawa
For this amount of load current and duty ratio I recommend a flyback topology. The maximum duty cycle of a boost is typically around 90% and the duty cycle needed for a boost topology to support this, not including any losses, is 85%. Once losses are added the duty cycle will increase.
The TPS40210 could be used as a flyback for this but as John said there are not any reference designs.
Do you have some details on the application you could share?
I looked at this a bit more and the boost topology may work though it is on the edge. Make sure they select a lower switching frequency to extend the off-time as much as possible to keep it above the minimum off-time limitation.
Hi Anthony-san,
Thank you for your response.
Applicaton is for TV backlight. If customer would like to evaluate, can TI support any EVM with reference design?
I'll visit customer tomorrow, if customer is interestisng in this, maybe they will request EVM.
Thank you for your advance
K.Narisawa
Typically that will come from design services group. Since this is TV application I suppose we can expect large volumes. They will require business case and detailed specifications to create the design. Are there other power needs that could also be incorporated into the design? It is ok to have multiple converters and outputs for these designs..