Hello,
i want to use the TPS63031 3V3 (fixed output) Buck/Boost Converter.
In my system there are a 5V (USB) and a 2V...3V input supply (2xNiMH) voltages. The TPS63031 is controlled by a MCU which can run from 2V...3.6V. In some cases the MCU needs regulated 3.3V and therefore enables the Converter but in other cases (e.g. low power modes or startup) it wants to be sourced directly by the 2V...3V battery without using (EN=pulled Low) the TPS63031. So what i need is a input pass-through. "Unfortunately" the TPS63031 does a "Load Disconnect During Shutdown".
I ask myself if one of the attached manual pass-through solutions (see picture) could work in this case.
Thanks for any help!