Hello,
I have the following question regarding the LM3481Q and LM3488-Q1.
- In the datasheet of the first the shutdown current is listed as 10µA in the key specifications, and 5µA in the description text (2nd paragraph), the FA/SYNC/SD pin description, and in the Frequency Adjust / Synchronization / Shutdown section. For the LM3488-Q1 it is listed as 5µA in the description and key specifications, and 10µA in the FA/SYNC/SD pin description and the Frequency Adjust / Synchronization / Shutdown section. Which number is correct and are the parts practically equivalent as far as the shutdown current is concerned?
- To increase the slope compensation the circuit shown for the LM3481Q (figure 22) and the one for the LM3488-Q1 (figure 25) have the positions of RSL and CSEN reversed. Is this correct and they are different?
Thanks for the help.
Belenie