Is it possible/acceptable to run the TPS54618-Q1 at a Vin = 6.5V "continuously"? The specification shows the ABS MAX for Vin = 7.0V and the "Operating Input Voltage" under "Electrical Characteristics" shows Vin = 2.95V to 6.0V.
I would like to know based on any data we have if it is possible to have the device running with a Vin = 6.5V for "long" durations. For example if the device is fed by another supply that typically outputs 6.0V but may have excursions up to 6.5V that last minutes or hours will this be OK for the TPS54618-Q1?
Kind Regards,
Marc