I'm designing a prototype power supply to using an LM5122. It's designed to work for a 18 - 28VDC input and a 24V 6A output, but for some reason both my mosfets go into short circuit as soon as the supply is enabled (as soon as the turn on threshold on UVLO is reached)
I've checked and double checked my design but I can't find out why. The mosfets should be able to handle up to 80V and 60A. This should be enough
The schematic (still prototype, could be neater)
Am I missing something why this is happening?
Hope somebody can help me with this.