Hello
My customer has question about TPS53318 OCP function.Coud you teach me about question.
Data sheet P19[Current Sense, Overcurrent and Short Circuit Protection]
「In an overcurrent or short circuit condition, the current to the load exceeds the current to the output capacitor
thus the output voltage tends to decrease. Eventually, it crosses the undervoltage protection threshold and shuts
down. After a hiccup delay (16 ms with 0.7 ms sort-start), the controller restarts. If the overcurrent condition
remains, the procedure is repeated and the device enters hiccup mode.」
When the OCP,Device is shutdown(latch-off)?Or hiccup mode?
Regards
TK