Hi Team,
I'd like to ask about TPS65261.
Our customer is going to use TPS65261 on the following condition.
◇Vin=10V-17V(4cell battery)
⇒Vout1=8V, Iout(max)=3A
⇒Vout2=1V, Iout(max)=2A
⇒Vout1=4.9V, Iout(max)=2A
However, It is not only can enter up to 5.5V in Webench.
Why can not I enter only up to 5.5V?
Could you tell me value of maximum output voltage of the TPS65261?
Best Regards,
Yusuke / Japan Disty