I understand that the TPS61220 does not have reverse input protection for the case where batteries are put in backwards. I have tried this and found that the TPS61220 gets very hot, but when the batteries are put in correctly the regulator goes back to working again. I see that the part has thermal overload protection. So will this always be the case, that it will go back to working after reversing the input, because of the thermal overload protection? Thanks in advance.