I have used a schematic generated by the TI website and made sure all the parts are as needed, wired on a pref-board. A the beginning the voltage went up to around 22V (supposed to be 30V), after a while the voltage dropped to the input voltage and the current limit on my bench power supply went off. After this, it always go to current limit when I power up. I checked pin #8 and I can see a square wave pattern but seems like it is going into shut-down and up again and continues to do that. Idea?