I am using the TPS62561 (the TSOT-23 package that does not have a mode pin) in a small design. It seems that when there is no load on the unit, it will drain the batteries (providing power to the TPS62561) faster than with a load on the unit.
I thought that the without the mode pin the PFM operation would be enabled all the time but it seems like the PFM is DISABLED in this package. And I do not see any comment on the DS about which way PFM is configured in this package.
(Unfortunately I haven't had a chance to scope it yet to check as the circuit is at another location.)
Any comments would are appreciated!
Thanks,
Kurtis Unger