Would like to use TPS62125 for 5.5V to -5V/300MA.
Can Iget recommended design as the webanch cant support it?
According to TPS62125 datasheet this scheme has to be:
BUT ACCORDING TO APPLICATIONE NOTE SLVA514 we saw:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The app note was updated more recently than the D/S, so use its circuit.
But the TPS62125 will not give 300 mA output as an inverter. I recommend the TPS62160 with its inverter app note on its product page instead.
Webench does not support the inverting configuration yet.
Any inverting buck-boost will have a reduced current as compared to the same buck converter circuit.
The circuit in the D/S says 150 mA. The app note is more conservative and gives 120 mA. The app note contains a detailed discussion of this circuit. Thus, the D/S refers to it.