Dear support,
I have some questions with TPS65217D.
1.as is shown in the picture,I want DCDC1 output voltage of 1.35v(LPDDR3 need), how to configure the value of capacitance and inductance?
2.Is DCDC2 able to connect all the loads(about 870mA) shown in the picture? if it is ok, how to configure the value of capacitance and inductance to get 1.8v?
3.what the max current of LDO3 and LDO4 is ?