This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54550- Efficiency for 1V output is very low.

Other Parts Discussed in Thread: TPS54550, SWITCHERPRO

Hi,

Am using TPS54550. For Vin=5V(4.5to5.5) ; Vout=1V (50mV ripple) ; Freq-700KHz, am getting a max efficiency of just 81% at for 4.7uH (Tunable).

Please help me in tuning the circuit to achieve a min of 85% effciency @ 1.27A; 2.32A and 3.016A.

Have attached the report, not sure whether its viewable.

TIA

5to1V0_DIGcore_Design_Max.pdf